Accessing previously saved projects
Troubleshooter project files save all data configuration and process models created on the data. Continuous Troubleshooter project files typically have a .csa file extension.
From within the Continuous Troubleshooter
-
Click on the File menu and select [Open], or click on the [Open] button in the toolbar.
-
Browse to the Continuous Troubleshooter project file to be opened. Continuous Troubleshooter projects have a .csa file extension.
-
Click [Open] to open the Continuous Troubleshooter project file.
Using the context menu within Windows
-
Browse to the Continuous Troubleshooter project file to be opened. Continuous Troubleshooter projects have a .csa file extension.
-
Right click on the file, and select [Open with...] from the context menu.
-
Select Continuous Troubleshooter from the recommended programs.
-
Click [OK] to open the Continuous Troubleshooter with the project already loaded.
Using the Command prompt
-
Type the directory where application is installed, the name of the application, and the project name into the command line. For example: C:\Program Files\Proficy\Proficy CSense "ProjectFile.csa"